See What the Textbook Can’t: Thermal Imaging in the Classroom

THE OBJECTIVE: MAKE PHYSICS VISIBLE

Heat is difficult to teach for one simple reason: most of the interesting part is invisible.

Students can learn that energy moves from warmer objects to cooler ones, that friction converts kinetic energy into thermal energy, or that different materials conduct heat at different rates. But understanding those ideas from a diagram is not quite the same as watching them unfold in real time.

That is where thermal imaging changes the lesson. Point a FLIR thermal camera at a motor, electrical connection, wall, cup of hot water, or simple classroom experiment and an abstract discussion about temperature becomes something students can observe, question, and measure. The theory is still there—it just has to answer to what is happening in front of them.

For educators, that creates a useful shift. Instead of asking students to imagine where heat is moving, they can ask them to watch it happen.

The question: Is the metal really colder?

Experiment One: Metal Strip vs. Wooden Spoon

Put a metal strip and a wooden spoon in the same room, then ask students to touch them. The metal will probably feel colder, which makes the obvious prediction equally obvious: it must be at a lower temperature.

Except it probably is not.

Two objects will typically be close to the temperature of their surroundings. The difference is thermal conductivity. Metal transfers heat away from a warmer hand much more readily than wood, creating the sensation of a colder surface even when the objects begin at roughly the same temperature.

Now hold both objects for a couple of minutes and look again with the thermal camera. Heat spreads along the metal, while the warming in the wood remains much more localized around the point of contact. A process that students might otherwise have to imagine can be watched as it unfolds.

It is a wonderfully simple experiment because the lesson begins with an everyday assumption, gives students evidence that challenges it, and then asks them to explain the difference. Science has, in effect, won an argument with a spoon.

CENTRAL CONCEPTS Thermal conductivity · Heat transfer · Insulation · Temperature vs. perception

The question: Where does the energy go?

Experiment Two: Rubbing Erasers, Hands, and Ice

Rub your hands together and nobody needs a physics degree to notice that they get warmer. What is harder to see is where that energy goes.

In a friction experiment, students rub their hands together, move an eraser across a rough surface, or work with an ice cube while observing the result with an infrared camera. The temperature increase makes the conversion of kinetic energy into thermal energy visible, and if students keep watching, they can follow the subsequent cooling as heat spreads through the materials.

Then the ice cube makes the experiment slightly less obedient. Some of the thermal energy contributes to melting the ice, while heat also conducts from the warmer table toward the colder cube, lowering the local temperature of the table surface.

One eraser, a pair of hands, and an ice cube have now opened a conversation about friction, energy transformation, conduction, cooling, and phase change.

Not a bad return from the stationery cupboard.

CENTRAL CONCEPTS Friction · Energy transformation · Phase change

The question: Which material really holds onto heat?

Experiment Three: Cups, Clothes, and Keeping the Heat In

A ceramic mug looks as though it should be better acquainted with hot water than a thin plastic cup. Ask students which will become hotter and there is a good chance the ceramic will win the vote.

The experiment gives them something more interesting to think about. The thin plastic cup quickly approaches the temperature of the hot water, while the ceramic mug warms more slowly. Wait a little longer, however, and the water in the plastic cup cools faster, helping students connect what they see with the insulating properties of the different materials.

The same principle can be explored with clothing. A thick outdoor garment does not need to appear hotter on the outside simply because it keeps somebody warm—good insulation slows the transfer of thermal energy.

With an infrared camera, students can compare temperature patterns across the water, the outside of the cup, and clothing surfaces rather than reducing the experiment to one number. They can even blow across the water and watch the surface cool.

The cup has not become more complicated. It has simply become much harder to dismiss as “just a cup.”

CENTRAL CONCEPTS Thermal properties of materials and objects · Heat conduction · Heat insulation

From Classroom Experiment to Trade-School Skill

The beauty of these experiments is that the science does not stop being relevant when the lesson ends.

Thermal cameras are used in real building, electrical, mechanical, and other technical applications. That makes the same principles explored with spoons, erasers, and cups particularly useful in trade schools and technical colleges, where students are preparing to work with systems in which heat can reveal how equipment and materials are behaving.

An electrical student can begin with the idea that resistance and operating condition affect temperature, then learn to compare thermal patterns across components. HVAC and building students can move from cups and clothing to insulation, heat loss, and building envelopes. Mechanical and maintenance students can take the same understanding of friction and heat transfer into the inspection of motors, bearings, and other equipment.

The equipment becomes more serious, but the habit of mind stays remarkably similar: make an observation, question what you are seeing, and work out whether the evidence supports the explanation.

There is also an advantage to learning this while still a student. A classroom or training workshop is a forgiving place to take a poor measurement, choose an unhelpful surface, or discover that the result is not what you expected. It is considerably better to learn why an inspection went wrong there than beside an asset where somebody is waiting for the answer.

ELECTRICAL

Compare thermal patterns across components and operating conditions.

HVAC + BUILDINGS

Compare thermal patterns across components and operating conditions.

MECHANICAL

Carry friction and heat-transfer concepts into equipment inspection.

FLIR Thermal Cameras in the Classroom: Downey High School

We brought the excitement of FLIR Thermal Cameras to Downey High School in Downey, CA.

Thermal cameras gave students the opportunity to learn about heat and temperature in an interactive and engaging way.