Train Through the Smoke: Building Firegound Confidence Before the Alarm

The middle of a vehicle fire is a fairly terrible place to discover what a button does.

Smoke has taken away the view, temperatures are climbing, the scene is changing by the second, and decisions need to be made long before anyone has time to consult a manual. Thermal imaging can give firefighters another way to see through that environment—but only when using the camera and interpreting the image have already become familiar.

That is why hundreds of women firefighters gathered in Tlaxcala, Mexico, for practical training designed to build exactly that confidence. Around 460 women from across the country attended Mexico’s Regional Firefighters Congress 2025, taking part in conferences, competitions, and hands-on emergency-response workshops that included thermography, fire investigation, and live vehicle-fire training.

For a profession in which women remain significantly underrepresented, the scale of the event mattered too. Figures suggest women account for fewer than 10% of firefighters globally and just 5.53% in Mexico. Here, however, hundreds of them were not standing on the sidelines.

They were on the fireground.

WOMEN IN FIREFIGHTING

<10%

WORLDWIDE


553%

IN MEXICO

01 TRAINING BUILT FOR THE REAL FIREGROUND

The congress brought together more than 450 women from across Mexico to strengthen skills in firefighting, rescue, and emergency response. Live demonstrations covered core techniques including vehicle firefighting, scene awareness, fire investigation, and the fundamentals of reading heat patterns under pressure.

02

SEEING MORE THAN SMOKE

Hands-on sessions gave participants the chance to work with FLIR K-Series thermal cameras in realistic scenarios. The goal was not simply to use the tool, but to understand what the image was telling them: where the heat was building, what obstacles were hidden, and how thermal information could support faster, better decisions.

03

CONFIDENCE IS PART OF THE EQUIPMENT

Thermal cameras do not replace training; they make good training more powerful. The event showed why hands-on practice matters: confidence grows when firefighters can connect the image on the screen to the reality in front of them. That confidence helps crews move more decisively in smoke, interpret heat more accurately, and use the technology as part of a disciplined response rather than a guessing game.

FLIR K85-N

“It was an honor to train these incredible women in the use of thermal imaging for firefighting—and to help build awareness of the daily dangers crews face and how this technology can support safer decisions.”


Teresa Gonzalez, Key Account Manager for Latin America, FLIR

MORE EXPERTISE. STRONGER RESPONSE.

Mexico’s investment in women firefighters is also an investment in capability. By supporting practical training and access to advanced thermal imaging, FLIR helped reinforce a simple idea: better tools, used well, create safer outcomes. The result is not only better visibility in the moment, but a stronger, more skilled firefighting community over time.