ACTIVE FIRE PREVENTION FOR ANCIENT ITALIAN FORESTS
Protecting Apulia with an advanced, 24/7 early fire detection system
The Ionian arch of Apulia is a region rich in history, stunning coastal landscapes, and ancient cultural traditions that reflect the harmony between nature and civilization. However, it is also particularly vulnerable to wildfires, especially during the summer season when high temperatures, dry vegetation, and increased tourist density heighten the risk.
Preventing and managing fire hazards is therefore a top priority to safeguard the environment, biodiversity, and the safety of both local communities and the many visitors who choose this beautiful area for their holidays.

To mitigate fire risks, the Apulia Region has implemented an Automatic Fire Outbreak Detection and Alert System. This system uses state-of-the-art, highly reliable technologies to detect fire outbreaks both preventively (detecting early warning signs) and during emergency situations, operating 24 hours a day and in all environmental conditions.
Following a successful initial deployment that helped monitor the natural environment of the Alta Murgia National Park, the early fire detection system has been expanded to protect the most valuable areas of the Ionian arc of Apulia. It uses the same core technologies, particularly Flir's high-sensitivity thermal cameras.
The Central Role of Infrared Sensors
At the heart of the early fire detection system are Flir PT-Series dual-sensor thermal cameras. These combine a thermal sensor and a visible light sensor on a high-speed, high-precision pan/tilt platform capable of continuously scanning the area for even the slightest signs of abnormal and potentially dangerous heat.
The cameras are mounted on elevated monitoring stations, each covering a detection radius of over 12 km and offering 360° surveillance. This ensures continuous protection in all conditions—from total darkness to full sunlight. Such a rapid response is critical to protecting the land from fire risks.
An Integrated Detection System Ensuring Responsiveness and Reliability
The early fire detection system in the Ionian arc of Apulia consists of six monitoring stations equipped with Flir thermal cameras, covering approximately 2,000 km² of forested land.
These stations are connected via a dedicated fiber optic and microwave radio network to a central hub that automatically collects and analyzes the thermal camera images in real time. This hub communicates any fire alerts to the Civil Protection Operations Center of the Apulia Region.
The communication network and real-time image processing system were developed by CAE, which acted as the system integrator for the entire project.
“We had already worked successfully with Flir on the previous fire detection project in the Alta Murgia National Park,” says Luca Papandrea, Operations General Manager at CAE. “Over the years, Flir’s thermal cameras have performed flawlessly, proving their reliability. So, for the new project protecting the Ionian arc, we chose Flir cameras again. Their innovative technical features even allowed us to submit an enhanced proposal compared to the original tender specifications.”

Complete Technological Solutions for Critical Area Protection
The integration of infrared thermal sensors and visible-spectrum electro-optical sensors with a robust pan/tilt mechanism is a key strength of the PT-Series thermal cameras. These systems reflect decades of Flir’s experience in developing optimized and highly reliable solutions for protecting critical areas across various sectors.
In addition to the thermal cameras, the fire detection system includes other security technologies from Flir to protect the monitoring stations from unauthorized access, ensuring comprehensive safety.
“Our ability to offer products, complete solutions, and technical consulting across the entire spectrum of critical infrastructure protection is one of Flir’s strengths,” Piracci emphasizes. “Our portfolio includes market-leading products, integrated into a holistic system that spans perimeter security to risk factor detection—such as early fire detection.
Preserving the Land for Communities and the Environment
The automatic early fire detection system in the Ionian arc of Apulia has proven to be reliable, minimizing false alarms and demonstrating high efficiency during interventions.
The exceptional thermal sensitivity of Flir’s PT-Series cameras enables timely detection of even the smallest outbreaks in any environmental condition. Meanwhile, the image processing software can predict the direction of fire spread, helping guide field response teams.
By combining advanced technology with specialized design and implementation expertise in protection and prevention, the system ensures peace of mind for a region of great cultural, economic, and environmental value.
This high-performance pan-tilt-zoom camera offers 640 × 512 resolution, a 4K visible-light imaging sensor, and 25× optical zoom.