Reimagining Infrared: Flir Scales Expertise and Simplifies Thermal Imaging Camera Inspections
The new Flir iXX-Series is a line of predictive maintenance tools that supports users at all levels—solving documentation, communication, and decision pains so they can do more with less.
In the high-stakes world of industrial maintenance, the pressure to keep operations running and prevent failures is constant, as is the need to do it all with fewer resources. But what happens when the tools meant to streamline inspections, such as thermal imaging cameras, require specialized training and expert interpretation?
Enter the Flir iXX-Series: a new breed of thermal camera that’s not just smarter—it’s strategically transformative. Powered by an ecosystem of mobile apps for condition monitoring, the iXX-Series is designed to democratize thermography, streamline workflows, and enable secure, scalable inspections across industries.
The Expertise Gap

Across manufacturing, utilities, and infrastructure, one challenge looms large: a shortage of skilled thermographers. In fact, 60% of maintenance teams say they don’t have access to technicians who are trained in thermography.
Professional condition monitoring with a thermal imaging camera requires expert training for consistent results. Thermographers need to understand how to properly set the camera, how to interpret results, and how to then provide reporting that accurately details each asset’s current state and potential need for repair.
The iXX-Series flips that model on its head. With app-guided workflows, even junior technicians can perform inspections with confidence. Safety instructions—such as warnings for dangerous work areas—onboarding tutorials, and remote support are built into the experience, allowing teams to scale their programs without sacrificing quality.
“Infrared cameras typically are only useful in the hands of those who have gone through thermography training and have months or years of experience. The iXX changes this—now new or inexperienced users can be guided through inspections with apps or remote support.”
—Rob Milner, Flir Director of Business Development

From Data Gatherers to Insight Generators
Of course, the iXX-Series isn’t just for newcomers: it’s also a powerful tool for seasoned thermographers. “It’s an opportunity for in-house experts to scale their knowledge," explains Flir's Rob Milner. "They go from data gatherers to program architects, from report writers to insight generators, from trainers to scalable mentors.”
Instead of travelling to a site and walking from asset to asset, expert thermographers can create inspection routes, embed safety instructions, and provide real-time guidance to a team of inexperienced thermographers—all through iXX integrated apps.
This shift transforms the role of the expert from data gatherer to program architect. They become mentors, insight generators, and strategic advisors who can support multiple technicians simultaneously and elevate the entire maintenance program.
Flir further supports this capability with the new AssetlinkTM app. This browser-based software comes installed on all iXX-Series cameras, allowing users to upload radiometric images, connect them instantly to an asset hierarchy, and include data for improved workflows and simplified reporting.
The cameras are also compatible with Flir Meterlink®,which allows you to monitor a variety of electrical and environmental conditions simultaneously for deeper analysis and use in reporting.
Security Meets Connectivity
The iXX-Series and Assetlink aren't just revolutionizing thermography: they're also improving cybersecurity. In an era where 43% of cyberattacks target manufacturing and critical infrastructure, connectivity can be a double-edged sword. Many organizations, including utility companies, hospitals, and government agencies, operate within tightly controlled IT environments, making wireless communication a challenge.
Flir addresses this challenge head-on, providing the support of an ISO 27001-certified company, so clients can rely on Flir to protect their data. Clients using the iXX can also deploy mobile device management or custom apps that ensure data security policies are followed. In addition, two iXX models feature LTE communication* as well as Wi-Fi. So whether it’s LTE-enabled cloud uploads or private, on-premises data handling, the iXX adapts to the environment—not the other way around.
*i35/i65 LTE models are currently not available in the US and Canada.

Apps that Work the Way You Work
Launching with several major third-party apps, the iXX-Series is built for flexibility:

Condoit is the single source of truth for electrical system layout and maintenance, enabling faster inspections, safer operations, and stronger customer relationships. With a digital platform that provides dynamic single-line diagrams, maintenance visibility, and NFPA® 70B maintenance records, this integration furthers the mission of Condoit to make the world’s electrical system safer and more reliable.

Thermidoc offers professional-grade but user-friendly reporting with built-in analysis tools. This app allows you to create inspections and describe your observations with text and images, both visual and thermal. Post-inspection, you can generate an impressive report in seconds.

Multisense 7313 combines vibration and thermal imaging data from Flir iXX devices to give users a clear picture of asset performance. The app allows instant creation of PDF reports that can be shared directly with teams, helping maintenance professionals track equipment health, prevent downtime, and improve efficiency.

Envelopeir, or eIR, is designed to streamline building envelope inspections—making high-performance building audits more efficient, especially on large projects. eIR reduces on-site time, improves trade accountability, enhances construction quality, and provides valuable data for architects and future projects.
And that’s just the beginning. Organizations can develop private apps tailored to their workflows, solving documentation, communication, and decision-making challenges with precision. As Milner explains, “One common pain is that users can’t use wireless communication on current Flir cameras because they need to work within their own company’s network. With the iXX, companies can deploy apps to ensure their inspections fit into their secure IT environments, connect to their preferred data management systems, conform to their workflows and support their new hires.”
Built for the Real World
The iXX-Series isn’t just smart—it’s rugged. With up to 480 × 640 thermal resolution, Flir’s patented MSX® image enhancement, and a 5-inch high-resolution touchscreen, the iXX cameras deliver crystal-clear imaging in the harshest environments. Drop-tested to 2 meters and rated IP54, they're ready for underground vaults, solar farms, coal plants, and building inspections alike.

The Bottom Line
The Flir iXX-Series isn’t just a new product line—it’s a new philosophy. It’s about scaling expertise, simplifying workflows, and empowering teams to make smarter decisions, faster. Whether you're a veteran thermographer or a technician just starting out, the iXX-Series offers a “made-for-me” experience that adapts to your needs, your environment, and your mission.
In a world where uptime is everything and insight is power, Flir’s iXX is more than a camera: it’s a catalyst for change.