How Thermal Imaging Is Helping Prevent EV Battery Fires Before They Start

Electric vehicles are changing the way the world moves, but behind every quiet motor and rapid-charge is a battery pack containing hundreds or even thousands of individual components.

Each cell, weld, connector, cable, and module must work together reliably. A loose connection, weak weld, leaking cell, or abnormal rise in temperature can reduce performance, shorten battery life, or create a serious fire risk.

The challenge for manufacturers is that many of these faults are difficult to see. A battery pack may appear perfectly assembled while a hidden electrical resistance point is already generating excess heat.

Thermal imaging changes that. By showing how heat is distributed across cells, modules, and electrical connections, thermal cameras allow manufacturers to identify small abnormalities earlier, strengthen quality control, and respond before rising temperatures become a dangerous event.

A Battery Pack Is Only as Strong as Its Weakest Connection

EV battery packs are built by combining smaller cells into modules and connecting those modules within a rigid structure.

Every mechanical and electrical connection must be secure. When a connection is loose, poorly fitted, or incorrectly welded, electrical resistance can increase. That resistance generates heat, reducing the efficiency of the battery and potentially creating conditions that could lead to failure or fire.

Visible-light inspection systems can confirm that components are present and correctly positioned. However, they cannot prove that electricity is flowing properly through the connection.

Reflective metal surfaces create another challenge. Glare, shadows, and changing illumination can make conventional visual inspection difficult, particularly when connectors are positioned deep within a complex battery assembly.

A component can therefore look correct while behaving incorrectly.

A thermal image of the interior of an EV

Uneven heating displayed by the lithium battery unit

See the Cell That Does Not Belong

—Thermal imaging identifies the one battery cell heating differently from everything around it.

Heat Reveals What Appearance Cannot

Poor electrical connections often produce a subtle rise in temperature long before they fail completely.

Thermal cameras detect that heat without touching the battery or interrupting the production process. Instead of assessing only the appearance of a connection, manufacturers can examine how it behaves when current passes through it.

A loose connector may appear hotter than neighbouring connections. A weak weld may create an uneven thermal pattern. A damaged cable or unstable load may produce a localised hot spot that would be invisible to an operator or visible camera.

This makes thermal imaging particularly valuable during validation and end-of-line testing, when manufacturers need confidence that the completed battery pack will perform safely and consistently.

Fixed thermal cameras, such as Flir A-Series Smart Sensor models, can be integrated directly into automated production and testing processes. Depending on the size and position of the battery pack, one camera may monitor multiple connections simultaneously.

Rather than checking one small area at a time, the camera captures temperature information across thousands of points throughout the scene.

Catching Thermal Runaway Before It Accelerates

Electrical connections are not the only source of risk.

Battery cells often retain some charge during assembly. When modules are connected, current may begin to flow between components, creating a normal increase in temperature. However, an internal fault, short circuit, damaged cell, or poor connection can cause heat to rise abnormally.

Under fault conditions, increasing temperature can accelerate internal reactions and generate still more heat. This self-reinforcing process is known as thermal runaway.

Left undetected, thermal runaway can damage the battery pack, endanger workers, interrupt production, and potentially cause a fire within the facility.

A Battery Management System can monitor the completed pack, but it may not be installed during the earliest stages of assembly. This can leave a gap in temperature monitoring precisely when cells and modules are first connected.

Fixed thermal cameras monitor the entire visible assembly continuously, reducing the chance that a developing problem will be missed.

A50/A70 Smart Sensor

Turning Thermal Data Into Operational Awareness

For many EV battery manufacturers, detecting a temperature anomaly is only the first step. Operators also need a way to monitor thermal conditions across multiple production areas, identify developing issues quickly, and understand how equipment is performing over time.

Flir United VMS (UVMS) helps bring thermal monitoring into a centralized operational platform. By integrating temperature data from Flir thermal sensors such as the A50/A70 and A-Series cameras, UVMS allows operators to monitor critical assets from a single interface.

Customizable dashboards, maps, and dynamic trend views help users visualize thermal conditions across a facility, while user-defined temperature alarms provide immediate notification when assets exceed expected operating limits. This enhanced situational awareness enables maintenance and production teams to identify abnormal conditions earlier and prioritize investigations before minor issues become unplanned downtime.

For large-scale manufacturing operations, UVMS also supports temperature trending and reporting, helping organizations analyze long-term equipment behavior and identify recurring patterns that may indicate developing reliability concerns. The platform's scalability allows thermal monitoring to expand across multiple production areas, facilities, or server-client environments while supporting organizations that require the cybersecurity and centralized management capabilities of a video management system.

Rather than viewing thermal data one camera at a time, operators gain a broader understanding of asset health across the production environment, helping support safer operations, improved uptime, and more informed maintenance decisions.

Safer Batteries Begin on the Production Line

Earlier fault detection can help manufacturers reduce end-of-line failures, improve production consistency, protect employees, prevent damage to facilities, and increase confidence in the finished battery pack.

It also helps move quality control away from occasional manual checks and towards continuous, repeatable monitoring.

As EV production grows, manufacturers will need testing systems capable of keeping pace without creating unnecessary contact, delays, or additional risk.

Thermal imaging provides a way to inspect electrical behaviour, monitor temperature, and identify developing faults while the battery remains on the production line.

The result is not simply a safer manufacturing process. It is better information, fewer missed defects, and greater confidence in the batteries that eventually reach the road.

Because the safest battery fire is the one detected while it is still only a temperature change.

T865 High-Performance Handheld Infrared Camera

One Camera. Thousands of Watchpoints.

—Every pixel becomes a temperature measurement, helping ensure critical hot spots are not missed.