Cold Chain Under Pressure: Reducing Leaks in Hot Conditions
As summer heat pushes food storage, transport cooling, and refrigeration systems harder, small leaks become more expensive. Thermal monitoring, acoustic imaging, and optical gas imaging help teams detect problems earlier, protect product quality, and support stronger refrigerant management.
THE SUMMER PRESSURE POINT: WHEN AMBIENT HEAT RISES, SMALL LEAKS BECOME BIG RISKS
Refrigeration is a quiet, continuous battle. In hot weather, condensers, chillers, cold rooms, and transport cooling units work harder just to maintain safe temperatures. A minor refrigerant leak can quietly erode cooling capacity, force longer runtimes, increase energy demand, and shorten the margin for error across the cold chain. In food and beverage operations, early visibility matters because lost cooling performance can quickly become wasted product, compliance risk , and avoidable cost.
Cold chain processes can account for up to 70% of a facility's electrical energy use.
Refrigeration energy use can rise up to 30% when faults of inefficiencies creep into operation.
Food waste carries an estimated $940 billion global economic impact every year.
With an estimated 1.3 billion tonnes of food lost to spoilage globally each year, protecting refrigeration performance is both an operational priority and a sustainability issue.
WHY LEAKS ARE SO HARD TO FIND
Leaks are often small, intermittent, and hidden inside complex piping, valves, fittings, and equipment housings. Many refrigerants evaporate quickly, which makes evidence disappear fast. Inspectors also contend with hard-to-reach assets, cramped plant rooms, and loud background machinery.
Traditional leak detection can be slow, disruptive, and expensive when teams need to dismantle equipment, halt operations, or rely on repeated manual checks.
That is why earlier visibility matters. The sooner a team can move from suspicion to evidence, the sooner it can intervene before performance loss becomes spoilage, downtime, or avoidable cost.

THERMAL MONITORING
Reveals abnormal temperature behaviour linked to insulation faults, deteriorating components, and declining refrigeration performance.

ACOUSTIC IMAGING
Detects the characteristic sound of minute refrigerant leaks, scans large facilities quickly, and works effectively in noisy environments.

OPTICAL GAS IMAGING
Visualizes certain refrigerant leaks directly and helps teams pinpoint the source faster across larger cooling assets.
Together, thermal, acoustic, and optical gas imaging help teams move from suspicion to evidence faster.
AIM ACT READINESS
EPA leak-repair rules under the AIM Act are raising expectations around refrigerant management. Since 1 January 2026, covered appliances with 15 pounds or more of HFC or certain HFC substitute refrigerant face leak-repair obligations. Applicable leak thresholds include 20% for commercial refrigeration and 10% for refrigerated transport and other covered appliances. Better detection supports fast repairs, clearer documentations, and stronger environmental stewardships.