HEAR THE WASTE

How Acoustic Imaging Turns Energy Loss Into Measurable Savings

Compressed air is one of manufacturing’s most useful utilities—powering tools, actuators, production lines, controls, and countless everyday processes. But it is also unusually easy to waste without realizing it. When a leak develops, electricity is still being used to generate the air, compressors are still working to maintain pressure, and production may continue as normal. The loss simply becomes part of the background.

Unlike water, escaped compressed air leaves no puddle on the floor. There is no plume of smoke, and in a busy production environment there may not even be a hiss that stands out above the surrounding machinery. The compressor simply works a little harder to replace what has disappeared—and the electricity meter keeps counting.

Acoustic imaging changes the conversation because it makes that invisible loss visible and, crucially, measurable. Instead of simply finding a leak, teams can locate it, estimate its flow and annual cost, document it, and decide which repair deserves attention first.

THE LEAK WITH A STANDING ORDER

Compressed air is sometimes called the fourth utility of manufacturing, but unlike electricity or water, it vanishes without leaving much evidence behind. A loose fitting, tired seal, or damaged hose can quietly leak for weeks while the compressor compensates in the background.

That compensation matters. As leaks accumulate, compressors run harder to maintain system pressure, increasing electricity use, maintenance demand, and operating cost. Estimates show that a typical site loses about $40,000 a year to wasted compressed air alone.

Put another way, a leak does not send an invoice. It simply keeps one running.

From finding the signal to checking the source: handheld acoustic imaging helps technicians investigate leaks directly at the asset.

40000

A typical site can lose ~$40,000 per year in wasted compressed air.

FROM HISS TO PRICE TAG

Acoustic imaging works by detecting the ultrasonic turbulence created as pressurized air or gas escapes through a small opening, then placing the source onto a visible image. In a noisy factory, where fans, presses, conveyors and pneumatic equipment are already competing for attention, that ability to separate useful ultrasound from ordinary background noise is what makes the technique practical.

The clever part, though, is not simply finding the leak. Modern acoustic cameras such as the FLIR Si2-LD can estimate leak rate and annualized cost.

That distinction also reduces dependence on experience alone. At Togo Seisakusyo, a Japanese automotive components manufacturer pursuing a 'Zero Air Leak Factory,' operators work in conditions noisy enough to require ear protection. The company reported that acoustic imaging allowed less-experienced operators to locate leaks quickly in an environment where finding the source had previously challenged even seasoned maintenance specialists.

Acoustic imaging makes an invisible leak visible, pinpointing the source while quantifying leak rate and estimated annual cost.

A list of 100 leaks is a maintenance problem. A ranked list with annual cost is a maintenance plan.

THIRTY MINUTES. $50,000+ ON THE TABLE.

A recent industrial demonstration shows just how quickly the numbers can become tangible. During a 30-minute walkdown with an Si2-LD, the team identified approximately $6,000 in losses and more than $50,000 in annualized savings opportunity. The inspection also produced a digital report for repair planning and verification, making the process easy to repeat as part of a monthly or quarterly maintenance routine.

Half an hour is shorter than many meetings about cost reduction. Here, it was enough time to put a dollar value on losses that had previously been disappearing quietly into the background.

Scale that thinking across 80+ facilities and the arithmetic becomes harder to ignore. The results of the demonstration estimates that even 20% adoption across the footprint could represent a multi-million-dollar annual impact.

Explore Si2-LD
30 MIN

walkdown

$6000

losses identified

$50000+

annualized opportunity

20%

adoption across 80+ sites could mean multi-million impact

FIXING 22% CHANGED THE METER

Finding every leak is satisfying. Fixing the right leaks is useful.

At a US automotive parts manufacturer, acoustic inspections found 68 compressed-air leaks. The company repaired just 15 of them, around 22%, and still recorded a 54.6 m³/h reduction in air use, equal to about 15%. The same repairs cut CO₂ emissions by 230.4 kg per day and delivered more than $4,000 in annual electricity savings.

If that daily CO₂ reduction were sustained for a full year, it would amount to roughly 84 metric tons. All from repairing fewer than a quarter of the leaks that had been identified.

That is why quantification matters. Maintenance rarely has unlimited time, people or budget. Knowing which leak is merely interesting and which one is quietly eating the energy budget makes prioritization considerably easier.

Air leak from a hose visualized with the Si-Series acoustic imaging camera.

Read the Case Study

ONE LEAK EVERY TWO AND A HALF MINUTES

Another manufacturing example shows what happens when scale meets speed. At a 6,500 m² facility, an acoustic inspection identified 155 compressed-air leaks in six hours, with estimated losses of about $11,000. That works out to roughly one leak every 2.5 minutes.

By the time somebody has made a coffee, the camera could have found four.

The projected return on the camera was four to six months, or about two service rounds. In a separate automotive inspection focused on specialty gases, five leaks were found in just 10 minutes; the calculated annual savings from those five leaks alone were approximately $12,500.

The point is not that every plant will reproduce the same numbers. It is that once the loss can be seen and priced, compressed air and gas leaks stop being vague efficiency problems and become specific maintenance decisions.

Calculate Your ROI