Hotspot or Red Herring? Five Thermography Mistakes That Can Change the Diagnosis
Thermal imaging has become remarkably accessible.
Cameras are sharper, easier to operate, and available at price points that would once have seemed improbable. Point one at an asset and, within seconds, invisible heat appears on screen.
That ease of use creates a slightly awkward illusion: that taking a thermal image and carrying out thermography are the same thing.
They are not.
A thermal camera collects infrared information. The person holding it still has to decide whether the image shows a developing fault, normal operation, a reflection, a measurement error, or simply the limitations of the equipment.
And sometimes the difference between those conclusions comes down to surprisingly small details.
The Infrared Training Center (ITC) identifies five common mistakes that can make an otherwise convincing thermal image tell the wrong story.

1.
Focus First. Diagnose Second.
A blurry photograph might still capture a perfectly good holiday. A blurry thermal image is less forgiving, because poor focus does not simply make the picture look untidy—it can affect the temperature measurement itself.
That matters in thermography because image quality forms part of the measurement process. Once a thermogram has been captured, missing detail cannot simply be restored afterwards. If the equipment has since been shut down, the operating load has changed, or the inspector has already left the site, recreating exactly the same conditions may not even be possible.
The ITC example makes the point particularly clearly. One image records a maximum temperature of 91.1°C (196.0°F); once the target is properly focused, the corresponding reading rises to 103°C (217°F)—a difference of 12.9°C (21°F) from the same target during the same inspection.
That is a sizeable change to introduce simply by sharpening the image, and a useful reminder that the first question in thermography should not always be, “How hot is it?”
Sometimes the more important question is, “Is my image good enough to answer that reliably?”


THE TAKEAWAY
2.
Same Target. Very Different Answer.
Thermal cameras do not simply point at an object and reveal its temperature. They interpret the infrared radiation reaching the detector, which means the information the operator gives the camera matters just as much as the image itself.
Object parameters such as emissivity need to reflect the composition and condition of the target, while the inspector must also consider the surrounding environment. Get those assumptions wrong and the camera can produce a reading that looks impressively precise, while being anything but reliable.
The ITC example shows just how dramatic that difference can be. With emissivity set to 0.60, the target measures 59°C (139°F). Change the emissivity setting to 0.30, and the apparent temperature jumps to 90°C (194°F).
Nothing about the target changed. The interpretation did.
That is one of the more dangerous characteristics of poor thermal data: it rarely arrives with a warning that the settings are wrong. It simply presents a number, often with enough decimal-point confidence to look entirely trustworthy.
Which is why a good thermographer does not ask only, “What temperature is the camera showing?” They also ask, “What assumptions produced that number?”

Ԑ = 0.60, 59˚C

Ԑ = 0.30, 90˚C
THE TAKEAWAY
3.
Sometimes the Hotspot Isn’t Yours
The next trap is one of thermography’s better optical illusions: reflections.
A thermal camera detects infrared radiation rather than simply “seeing heat”, and shiny or low-emissivity surfaces can reflect radiation from other objects in the environment. That reflected energy can appear on screen as a convincing thermal anomaly, even when the target itself is behaving normally.
The ITC images show how easily this can happen. A bright area may look like an obvious hotspot until the wider scene reveals that the camera is actually seeing energy reflected from somewhere else.
The camera has not made a mistake. It has accurately detected the infrared radiation reaching its detector. The error comes when the operator assumes that all of that radiation originated from the target.
That is why thermography requires an understanding of radiation science and heat transfer, not simply an ability to recognise the brightest colours on screen. A skilled thermographer asks whether the pattern makes physical sense, what else in the environment could be influencing the image, and whether the apparent anomaly really belongs to the asset being inspected.

Ԑ = 0.60, 59˚C

Ԑ = 0.60, 59˚C
THE TAKEAWAY
4.
Small Difference. Big Consequence.
Thermal inspections naturally draw the eye towards dramatic temperature differences, but not every serious problem arrives in white-hot technicolour.
Shiny metallic surfaces can make meaningful temperature differences appear far smaller than they really are. Copper busbars are a good example because their low-emissivity surface can make reliable measurement difficult and, in turn, influence how a thermographer judges the severity of a developing fault.
The ITC example tells the story particularly well. Measured directly on the bare metal, the apparent Delta T between two points is just 2.3°C (4.1°F). Measure the same condition using electrical tape as the appropriate high-emissivity surface, and the Delta T rises to 45°C (81°F).
That is quite a leap from “probably worth keeping an eye on” to “perhaps somebody should deal with this now”.
The equipment did not suddenly become more dangerous when the tape was applied. The underlying condition was already there; the measurement simply became far more representative of what was actually happening.
And that is the important lesson: in thermography, a small apparent temperature difference does not always mean a small problem. Sometimes it means you need a better way to measure it.

Bare Metal: 2.3˚C (4.1°F)

Electrical Tape: 45˚C (81°F)
THE TAKEAWAY
5.
The Wrong Camera Can Make the Right Problem Invisible
The operator is not the only variable in a successful thermal inspection. Sometimes the camera itself is simply not the right tool for the job.
Thermal cameras vary in resolution, optics, and thermal sensitivity, and those differences determine how much useful detail an inspector can see and reliably evaluate. Higher-resolution cameras can distinguish finer features that may be difficult to resolve with fewer detector pixels, while lens choice becomes equally important when working distance and target size change. A wide-angle lens may be ideal for examining a large area at close range, whereas a telephoto lens can help resolve a smaller target from further away.
The building and powerline examples supplied by ITC make the difference particularly clear. In the lower-detail images, the overall thermal pattern is visible, but individual features are much harder to distinguish. In the higher-detail versions, structures and components become far more clearly defined, giving the thermographer more information on which to base an assessment.
That leads to one of the most useful questions to ask before an inspection even begins: “Do I have enough pixels on the thing I actually need to measure?”
The answer is not necessarily to buy the most expensive camera available. More capable equipment cannot compensate for poor inspection technique, just as excellent technique cannot recreate spatial detail that the detector never captured. The real skill lies in understanding the inspection, the target and the conditions well enough to match the right technology to the task.


THE TAKEAWAY
A Thermal Image Is Evidence, Not a Verdict
These five mistakes may look very different—poor focus, incorrect parameters, reflections, misleading surface measurements, and unsuitable camera choice—but they all point to the same underlying lesson: seeing something on a thermal image is not the same as understanding it.
A competent thermographer needs to understand not only how the camera works, but how heat behaves, how the asset operates and which environmental or measurement factors could influence the result. Just as importantly, they need the confidence to question what appears on screen rather than treating every bright area as an automatic diagnosis.
Formal training helps build exactly that discipline. ITC describes the aim as giving thermographers the knowledge to trust the accuracy of their measurements, carry out inspections safely and efficiently, strengthen the credibility of their findings, and improve the return from a thermography program.
The technology can make hidden heat visible. The expertise lies in deciding whether that heat is significant, what is causing it and, ultimately, what should happen next.